Issue
Cannot change the passwords for the BMENOC0311 using Web Designer.
Product Line
Ethernet Module M580
Environment
BMENOC0311
Resolution
The selection for changing the password on the target security window is greyed out and not selectable.
Due to cyber security reasons, the ability to change the passwords for BMENOC0311 Factorycast HMI module using
Web Designer is not allowed. Changing of the passwords for the BMENOC0311 Factorycast HMI module must be
performed from the 'Setup' web pages.
Опубликовано для: Schneider Electric Казахстан