Чем мы можем помочь сегодня?

About ZART8L, If I want to change remote device but I am still using same base station, new remote device should be download existing setting from configuration software?

If you want to use another Remote you need to program it with the Base ID address and right configuration, actually when the Remote has a Base ID address during the first connection it will send its configuration to the Base