Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
According to datasheet, operating distance is "50m", and maximum sensing distance is "100m". What is a difference between these distance explanation?
We speak about 100m in free field, we can guaranty a well functioning at 50m in industrial applications, actually it depends mainly of where the system is installed, for the moment no customer is complying about low range.