Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Are replacement parts available for the ATS46?
Issue:
Customer needs to replace the ATS46 control board and keypad.

Product line:
ATS46, Altistart 46

Environment:
All

Cause:
Product inoperative

Resolution:
The ATS46 went obsolete in January of 2004.  Replacement parts are no longer available and the customer should consider updating to current product.