Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Does the Modicon M241 HSC support periodic meter measurement?
Issue
Does the Modicon M241 HSC support periodic meter measurement?

Product Line
Modicon M241 PLC

Environment
HSC (High Speed Counter) feature in PLC

Resolution
Yes, the Modicon M241 controller supports up to 2 channels using the Fast input that can be setup as period meter.
Periodic measurement calculates the period between two events.