Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Where can I monitor motor voltage on an ATV71?
Issue:
Monitoring motor voltage on an ATV71

Product Line:
ATV61, ATV71

Environment:
All models and serial numbers

Cause:
Customer would like to monitor the motor voltage while the drive is running.

Resolution:
The motor voltage can be monitored by going to menu 1.2 Monitoring in the drive menu.