Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
What are the replacement fan assemblies for the ATS48 soft starters?
Issue:
Fan assemblies replacement for the ATS48

Product Line:
Altistart 48  ATS48

Environment:
All models

Cause:
Replacement

Resolution:
The replacement fan assembly is selected based on the ATS48 part number.
The largest units have multiple assemblies per ATS48.
See the attached file.

Schneider Electric Казахстан

Вложения
ATS48 Fan Assembly.pdf [188.7 KB]