Issue:
Reverse the rotation of an ILS motor
Product Line:
Lexium ILS motor
Resolution:
Reverse the rotation of an ILS motor
Product Line:
Lexium ILS motor
Resolution:
To reverse the direction of the ILS motor, you need to change the rotation parameter:
In LexiumCT, the parameter is Motion.invertDir (0 = clockwise 1 = counterclockwise)
You can also access this parameter by writing to its CANOpen address 28:6
The 2 cables needed to connect with LexiumCT are VW3L1T000R30 and TCSMCNAM3M002P
Опубликовано для: Schneider Electric Казахстан