Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
How do I access missing menus under the Main Menu on a ATV600/ATV900 Process Drive?
Issue:
Accessing missing menus under the Main Menu on a ATV6xx/ATV9xx Process Drive

Product line:
ATV600 and ATV900 series

Environment:
all

Cause:
Trying to program an ATV930 drive but it only provides access to the Simply Start, Dashboard, Diagnostics and My Preferences menus.

Resolution:
Factory setting on the drive is Basic Access Level.

To increase your Access Level:
Under the Main Menu, go to [My Preferences] -> [Access Level] and change to Standard or Expert.
This will allow access to the [Display], [Complete Settings], [Communication] and [File Management] menus.