Чем мы можем помочь сегодня?

what is the rated Current For the Contactor LC1D09 if it works on AC1 Loads ?

The rated current for the contactor LC1D09 on 380 V AC if works with loads of type AC1 is 20 A