Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Video: How do you access the fan and IGBT diagnostics menu on the ATV630 and ATV930 drives?
Issue:
Accessing the fan and IGBT diagnostics menu on the ATV630 and ATV930 Process Drives

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Need to run the auto IGBT or the Fan diagnostics for troubleshooting

Resolution:



Main menu
Complete settings
Maintenance
Diagnostics

Choose:
Fan Diagnostics
LED Diagnostics
IGBT Diagnostics with motor
IGBT Diagnostics without motor