Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
What is the part number for the DeviceNet Fieldbus Module for the Altivar Process Drive?
Issue:
What is the part number for the DeviceNet Fieldbus Module for the Altivar Process Drive?

Product Line:
Altivar Machines, Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
Part number required to order part

Resolution:
Altivar 600/900 Series
Part Number - VW3A3609