Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
DUP2 Does Schneider Electric offer the Berger Lahr EXRDM3913/50NEA motor or a suitable replacement?
No, the Berger Lahr EXRDM3913/50NEA motor with ID number 52951045500 is a special customized version for the company W&H.
This type is proprietary and is reserved for the company W & H and can not be purchased from Schneider Electric.
The customer must contact the OEM machine builder Windmuller & Holscher for a spare EXRDM3913/50NEA motor with ID number 52951045500.