Issue
Is the BMXPRA0100 compliant with security notification SEVD-2017-048-02?
Product Line
BMXPRA0100
Environment
Windows 10
Resolution
Is the BMXPRA0100 compliant with security notification SEVD-2017-048-02?
Exec firmware version 2.9 is compliant with SEVD-2017-048-02.
Only PV version 12 and above is compliant.
Is the BMXPRA0100 compliant with security notification SEVD-2017-048-02?
Product Line
BMXPRA0100
Environment
Windows 10
Resolution
Is the BMXPRA0100 compliant with security notification SEVD-2017-048-02?
Exec firmware version 2.9 is compliant with SEVD-2017-048-02.
Only PV version 12 and above is compliant.
Опубликовано для: Schneider Electric Казахстан