Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Is there an option to use a real key to lock out the ATV630 Process drives keypad?
Issue:
Is there an option to use a real key to lock out the ATV630 keypad?

Product Line:
Altivar ATV630 drive

Environment:
All

Cause:
Wants to use a real key to lock out the HMI pad on the ATV630 drive.

Resolution:
There is not a way to lock out the HMI with a external key on the ATV630 process drive.