Type 2 coordination is not possible with ATS22 due to the soft starter internal design of power semiconductor & its internal by-pass . Only table for coordination type 1 is available in the catalog. Attached pdf pages for type 1 coordination .
Опубликовано для: Schneider Electric Казахстан