Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
How can you copy an ATS22/ATS48 program from one soft starter into another one?

Article available in these languages: Испанский

Issue:
Is it possible to transfer the settings from an old ATS22/ATS48  soft starter to a new or replacement identical softstart?

Product Line:
Altistart Soft Starters

Environment:
All Models ATS22 and ATS48

Cause:
Adding or Replacing an ATS22/ATS48

Resolution:
If you have a laptop available, you can copy the settings from an old ATS22/ATS48 assuming it is still in working condition using the SoMove software to download the settings to your PC then uploading them back to your new ATS22/ATS48

You will need to download SoMove (Free)
https://www.se.com/ca/en/download/document/SoMove_FDT/

The required libraries for the ATS22/ATS48
https://www.se.com/us/en/download/document/Altistart_DTM_Library/

You will need to buy or use the Modbus cable TCSMCNAM3M002P

After successfully connecting the existing ATS22/ATS48
  • Save the project as a PSX file on your computer.
  • Now Connect to the new ATS22/ATS48 to SoMove
  • Open the project you saved earlier and upload it to the new ATS22 or ATS48 softstart.

If you are having issues connecting to your ATS22/ATS48 check the link below for troubleshooting
https://www.se.com/ca/en/faqs/FA313062/


Note: Both the old and the new soft starters have to be identical otherwise you can not copy the settings from one another without some modifications of some parameters or manually making the changes.