If you are unable to set date and time of IMU with Compact NSX/CompactNS/Masterpact NT/NW then please check the firmware version of the BCM ULP through Ecoreach Firmware Upgrade. If the firmware version of BCM ULP is 3.0.4 consider changing the firmware version of the BCM ULP to firmware version 3.0.7.
Опубликовано для: Schneider Electric Казахстан