Issue
The purpose of this Resolution is to inform Advantys users that the Ethernet NIM Web page firmware has been updated to version 1.14.2.
Product Line
Advantys STB
STBNIP2311
Resolution
Upgrading the STBNIP2212 Ethernet NIM web pages to version 1.14.2 adds support for the following modules:
- STBACI0320
- STBACI8320
- STBACO0220
- The web page 'Upgrade Procedure'
- Upgrade.exe application file
- Web file: web_files.zr
Please read the 'Upgrade Procedure' in the Attachments before attempting to load the web file.
Опубликовано для: Schneider Electric Казахстан