Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
How does the points capacity allocate when routing function is implemented in BMXNOR0200
Question:
How does the points capacity allocate when routing function is implemented in BMXNOR0200?

Answer:
If customer is using routing function(forwarding function), the points counts should include both client side & sever side. So customer have to use half of capacity points(3500) at either client side or sever side.