Floor standing drives ATV630 and ATV930, (ATVx30CxxF) are manufactured in Spacial SFN enclosure.
Enclosure dimensions of ATV930C31N4F are 600mm (width) and 600mm (depth), height is 2150mm (2000mm enclosure + additional 150mm fan)
It is possible to add plinth and its references can be selected from Spacial catalog.
Full catalog downloadable from web (link below)
https://www.se.com/uk/en/download/document/UEMKCAT012EN/
For ATV930C31N4F (and ATV630C31N4) it is possible to select plinth in 100mm or 200mm height.
Опубликовано для: Schneider Electric Казахстан