Issue:
Parameters to adjust when powering multiple ATV930 drives straight to the DC bus with a common DC power supply.
Product Line:
Altivar 930
Environment:
All
Cause:
Powering ATV930's with a single common DC power supply
Resolution:
1. Set your Access Level to Expert:
2. Set DC Bus Source Type to Supply Unit REC:
Parameters to adjust when powering multiple ATV930 drives straight to the DC bus with a common DC power supply.
Product Line:
Altivar 930
Environment:
All
Cause:
Powering ATV930's with a single common DC power supply
Resolution:
1. Set your Access Level to Expert:
- [My Preferences] -> [Access Level] -> [Expert]
2. Set DC Bus Source Type to Supply Unit REC:
- [Complete settings] -> [Generic functions] ->[dbS] ->[dCbS] ->[Supply Unit REC]
Опубликовано для: Schneider Electric Казахстан