Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
[Video] How to Install the nodes from Node Red web site into the HMIBSC?
Goals and Symptoms
The Magelis Edge Box HMIBSC running with Linux is supplied with Node Red and only the standard nodes are preinstalled by default.
In some cases, the user needs to add some specific nodes in order to design his application.
These nodes can be downloaded from Node Red web site or another server.
The goal of this resolution is to provide the steps to follow in order to install some nodes into the server.
Causes and Fixes
Here is an example to show how to install the OPC UA nodes