Issue
While running Power SCADA Operation version 8.2, customer sees the error in Runtime Manager: Software Protection Failure Error. No key found or no license available from network.
Product Line
EcoStruxureTM Power SCADA Operation 8.2
Environment
SCADA
Resolution
Install at least PSO 8.2 CU 6.
The installation files and other documents can be found in the link below:
https://community.se.com/t5/EcoStruxure-Power-Operation/v2020-Release-amp-Updates-Install-Procedure/td-p/186330
Опубликовано для: Schneider Electric Казахстан