Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Which Miniature Circuit Breaker protection devices need to be installed with EVlink Pro AC ?
The charging station shall be protected by the following devices (provide this set of protections for each socket):
Circuit Breaker 40A Curve C for each socket 7.4 kW (1P+N) or 22 kW (3P+N)
Circuit Breaker 20A Curve C for each socket 11 kW (3P+N)
Consult the Installation Guide (ref: NNZ1940301 or JYT24398) available on se.com.