Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
ATV340 and ATV930 Multidrive Load Sharing function capacity.
Issue:
How many Clients can you have with ATV340 and ATV930 Multidrive Load Sharing function?

Product Line:
Altivar 930, Altivar 340

Environment:
All

Cause:
Multiple motors on a Conveyor

Resolution:
On ATV340 or ATV930 with embedded Multidrive Client/Server load sharing function through Ethernet, we can have up to 10 Clients + 1 Server.