Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
What can cause an Arithmetic error/Overflow exception with CPU fault code( %SW125=16#DEF2) reported in Unity Pro/EcoStruxure Control Expert?
Issue:
Cause of an Arithmetic error/Overflow exception with CPU fault %SW125=16#DEF2


Product Line:
EcoStruxure Control Expert


Resolution:
If an Arithmetic operation such as a multiplication, addition etc. is performed and the result of the operation exceed the max value for the variable type, this will generate an Arithmetic error/overflow exception. %S18 will turn on and stay on until the cause of the error is cleared. In the example below, IN1 and IN2 when multiplied the result is 40000. This exceed the max value of 32767 for a INT data type and thus the cause of the error.
image