Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
V221-Slave mode installation
Issue
In application of multiple central units in Arc system, the error code XX-10 always appeared on Slave mode V221 even after execution of install command and Error reappeared again after few minutes from clearing error code on Slave mode V221.
_____________________________________________________________
Product Line

Arc protection relay
_____________________________________________________________

Environment
N/A
_____________________________________________________________
Root Cause
Customer didn’t follow the instruction in our V221 manual.
_____________________________________________________________
Solution
We have to follow the instruction in our V221 manual as shown in below screenshot.

1

1

_____________________________________________________________

=====End of document=====