Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Static IP configuration from the serial console appears to not persist after a reboot if a network is not connected.
Issue:
Static IP configuration from the serial console appears to not persist after a reboot if a network is not connected.

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755

Cause:
If you do not have a network cable attached to the NetBotz 750 or 755 and you serially provide it an IP and subsequently reboot the unit, the unit will appear to have no IP set to the public LAN.

Resolution:
Simply connect the appliance to the network and the IP configuration should reappear as configured. It is not lost, it is simply not shown when no network is connected.