Чем мы можем помочь сегодня?

Control Expert install returns error 'Installation of a sub component was aborted'.

Installing Control expert fails and returns the following error.
error
The sub components are located in the folder named '...:\ISSetupPrerequisites'.

The issue can be resolved by performing the following steps:

  • Run a registry cleaner
  • Reboot.
  • Open\mount the Control Expert installation iso file.
  • Reinstall all of the sub components found in the folder named '....:\ISSetupPrerequisites'.
  • Reboot.
  • Retest.

dir

Schneider Electric Казахстан

Вложения
RegClean.7z [255.84 KB]