How can we help you today?

Datasheet for configured/complete Compact NS Molded Case Circuit Breakers and Switch-Disconnectors

A configured/complete NS MCCB by minimum requirement should include below components:

1) Breaker Frame
2) Trip unit
3) Top Connection
4) Bottom Connection
5) Chassis (if withdrawable)

For configured Compact NS MCCB, we only have a readily available datasheet for the following:

A) Front-connected NS630b to NS1600 Fixed type Manually Operated with Micrologic 2.0 control unit
B) Front-connected NS630b to NS1600 Fixed type Manually Operated with Micrologic 5.0 control unit
C) Front-connected NS630b to NS1600 Fixed type Manually Operated with Micrologic 2.0A control unit
D) Front-connected NS630b to NS1600 Fixed type Manually Operated with Micrologic 5.0A control unit
E) Front-connected NS630b to NS1600 Fixed type Manually Operated Switch-disconnector

You may refer to Compact NS Catalog link below pages 161-162 of 194.

https://download.schneider-electric.com/files?p_Doc_Ref=LVPED221008EN&p_enDocType=Catalog&p_File_Name=LVPED221008EN.pdf

Example is C080N320FM for Front-connected NS800 3 Pole Fixed type Manually Operated with Micrologic 2.0 control unit

For other references you may refer to the Compact NS catalog for the electrical specifications, dimensions and etc.

For clarifications please reach out to Customer Care Center via:

SE Malaysia -> https://www.se.com/my/en/work/support/

SE Philippines -> https://www.se.com/ph/en/work/support/

SE Singapore -> https://www.se.com/sg/en/work/support/

Schneider Electric Malaysia