How can we help you today?

Operating Temperature Range for the 9065 Solid State Overload Relays

Issue:
Checking on the 9065 solid state overload relay operating temperature range.

Product Line:
Class 9065 Type S Solid State Overload Relay

Environment:
NEMA Contactors and Starters

Resolution:
The operating temperature is from -25 to +70 degrees Celsius.
Note: If overload relay is used in conjunction with the NEMA rated contactor, the contactor is rated 0 to +40 degrees Celsius.