Issue:
Are the bimetallic units in the GV starters replaceable?
Product Line:
IEC Contactors and Starters
Environment:
GV Manual Starters and Protectors
Cause:
Maintenance
Resolution:
The overload bimetal elements are not replaceable on these type starters, replace the complete unit only.
Released for: Schneider Electric Nigeria