Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the ohmic value and average power for the resistor used in the VW3A66713 dynamic brake kit?
Issue:
Ohmic and power value for resistor used in the VW3A66713 dynamic brake kit

Product Line:
Altivar Drives

Environment:
All

Cause:
NA

Resolution:
The value is  of the resistor is 28 ohms and the power is 204 watts.