Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the ATS48 soft starter that has a part number that ends in Q versus one that ends in Y?

Article available in these languages: Thai

Issue:
Difference between the ATS48 soft starter that has a part number that ends in Q versus one that ends in Y.

Product Line:
Altistart ATS48

Environment:
All serial numbers

Cause:
Customer in US is looking for an ATS48M10Q.

Resolution:
The ATS 48 ``Q`` was made for sale every where except the US.  It has 2 CT`s and a max voltage of 400 vac. The ``Y`` series has 3 ct`s and a max voltage of 690 vac.
If replacing an ATS48Q with a Y, it is very important to determine the full load amp rating of the motor. The ATS48**Q can be connected to the motor ``inside`` the Delta. This greatly reduces the amperage on each phase of the soft starter, allowing a smaller unit than normal to be applied to a motor. This is not currently possible with the ATS48**Y soft starters.
See the attached manual pages 92 to 94 (pages 11 to 13 of the electronic document)

Schneider Electric Nigeria

Attachment(s)
ATS48 Delta Motor wiring connections.pdf [23.71 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings