Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the NEMA rating for the XACA pendant station enclosure?
Issue:
NEMA Rating of the XACA Pendant Station

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony XAC Medium-Duty Pendant Stations

Resolution:
It is rated NEMA 4, 4X (indoor and outdoor), and IP65.
Pistol grip NEMA 4, 4X (indoor), and IP65.