Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an StF fault on the ATS48 Soft Starter?
Issue:
Remedy for the StF fault

Product Line:
ATS48

Environment:
StF faults

Cause:
n/a

Resolution:
The StF is a fault indicating Excessive starting time. As of December 2004, this fault is not documented in the United States Literature for the ATS48.
To remedy the fault perform the following:
* Check the mechanism (wear, mechanical play, lubrication, blockages, etc.).
* Check the value of tLs setting in the PrO menu.
* Check the sizing of the starter-motor in relation to the mechanical requirement.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings