Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the latch bar rivets for the Class 9423 Type M door closing mechanisms?
Issue:
Latch Bar Rivets for the Class 9423M3, M4, M9, M23 and M24.

Product Line:
Operating Mechanisms,Disconnect Switches, and Door-Closing Mechanisms

Environment:
9423 Door-Closing Mechanisms

Resolution:
The door closing mechanisms are supplied with the 31008-124-01 rivet(s) as standard. For replacement purposes order as outlined below:

9423M3 and 9423M23; requires (1) 31008-124-01 rivet.
9423M4, 9423M9 & 9423M24; requires (2) 31008-124-01 rivets.