Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is included with the Class 9998 Type S contact kits?
Issue:
9998 contact kit parts

Product Line:
Type S Accessories and Components

Environment:
Contactor and Starter Replacement Part Kits

Resolution:
The 3 pole contact kit will contain - 3 moveable contacts, 6 stationery contacts and 6 stationery screws.
***Springs are not included because part of the contact carrier assembly.

NOTE - 1 pole contact kit is 1 set of NO power pole contacts
- 2 pole contact kit is 2 moveable contacts and 4 stationary contacts with screws
- 4 pole contact kit is 3 moveable contacts and 6 stationary contacts with screws plus a set of NO power pole contacts.  The 4th pole power contacts are different from the normal starter contacts.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings