Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many drive configuration files can be stored in the ATV71 keypad?
Issue:
Storing drive configuration files in the ATV61 / ATV71 keypad.

Product Line:
ATV61 ,ATV71

Environment:
All

Cause:
Ffiles stored in keypad

Resolution:
The keypad can store up to 4 files.
To access and manage these files: Go to menu 1.12 (FACTORY SETTINGS) (FCS-)
See programming manual for details, if needed.