Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between XBTZ925 cable and XBTZG925 cable.
Following are the difference between XBTZ925 cable and XBTZG925 cable:
1. XBTZ925A and XBTZ925B, in connection with TSX CUSB45 converter, is used for programming HMI terminals: XBT N/R.
2.  XBTZG925 is programming cable for XBT GT11xx series HMI terminals only (Serial Tool port).