Issue:
Wants to use Altivar 61 or Altivar 71 drives on delta power system.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Needs to know if the RFI filter needs to be deactivated when using a corner grounded delta system?
Resolution:
As long as the input voltage remains within the normal range there should not be a problem.
This should be treated the same way as an impedance grounded system.
Remove the jumper to the left of the power terminal.
See the section of the installation manual for Operation on an IT (Isolated or impedance grounded neutral) system for details.
See the drives installation manual for more information and location of the RFI's filter tab.
See the attachment for the low horsepower ATV61 and ATV71 drives.
Wants to use Altivar 61 or Altivar 71 drives on delta power system.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Needs to know if the RFI filter needs to be deactivated when using a corner grounded delta system?
Resolution:
As long as the input voltage remains within the normal range there should not be a problem.
This should be treated the same way as an impedance grounded system.
Remove the jumper to the left of the power terminal.
See the section of the installation manual for Operation on an IT (Isolated or impedance grounded neutral) system for details.
See the drives installation manual for more information and location of the RFI's filter tab.
See the attachment for the low horsepower ATV61 and ATV71 drives.
Released for: Schneider Electric Nigeria