Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Boot-up Time of Altivar61/71 Drives on Power Up.

Article available in these languages: French, Dutch

The Boot-up Time of Altivar61/71 on Power Up (switch-off/switch-on) is approximately 2 seconds.

During this time, following processes take place inside the drive:
1. Charging of the capacitors.
2. Initialization of the internal switch mode power supply.
3. Initialization of the microprocessor
4. Reading of the EEPROM.
5. Synchronization of the microprocessors.