Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When does the cooling fan of Altivar 71 Drive start.

In Altivar 71 drive from frame Size 2 to 5b the fan starts on a temperature Threshold (THD) = 70%.

And from frame Size 6 to 15 the drive cooling fan starts as soon as the run command is given.

Refer the attachment for the KW details of Altivar 71 Size 2 to 5b and Size 6 to 15.

Schneider Electric Nigeria

Attachment(s)
ATV 71 Size Table.pdf [150.22 KB]