Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you unlock the access of all Drive Parameters in an Altivar 31 Drive

In order to gain access to all the Altivar 31 Drive parameters one of the two conditions will apply:

1. Parameter Access Via Standard Keypad (Integrated LED Display):

Enter the Customer password in parameter Terminal Locking Code (Cod) in Monitoring Menu (Sup).

2. Parameter Access Via Remote Keypad:
a. Enter the Customer password in parameter Terminal Locking Code (Cod) in Monitoring Menu (Sup).
AND
b. Set the Dip Switch called ‘Access Locking Switch’ at the rear portion of the Remote Keypad to ‘Unlock’ position. Refer to the attachment.
Note:
Customer password protection has priority over the switch setting.
Note:
In case the Customer set password is forgotten use the Master password ‘6969’ which resets the customer password and opens access to all parameters.

Schneider Electric Nigeria

Attachment(s)
1.jpg [23.9 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings