Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you get an external keypad on a NEMA 3R E-FLEX drive?
Issue:
External keypad option for E-Flex Nema 3R drive

Product Line:
Altivar Machines

Environment:
NEMA 3R only E-Flex drives

Cause:
Needs to order an NEMA 3R -E-Flex drive with a remote keypad display mounted on the door.

Resolution:
The E-Flex drive is obsolete. External keypad was not available on the E-Flex. The replacement ATV660 drive also does not have an option for external keypad on Nema 3R, as they are not UV protected.

Schneider Electric Nigeria

Attachment(s)
30072-454-01.pdf [6.36 MB]
E-Flex_30072-451-51.D.pdf [5.87 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings