Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a TVSS unit catalog number TVS4EMA16A compliant with specification UL1449 3rd edition?
Issue:
Is a TVSS unit catalog number TVS4EMA16A compliant with specification UL1449 3rd edition?

Product Line:
TVSS.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes, a TVSS unit TVS4EMA16A has a UL1449 3rd edition listing, and has an identification sticker on the inside of the unit that indicates this.
NOTE: The TVS4EMA16A is obsolete and replaced by the SSP04EMA16 (in a NEMA 1 enclosure or SSP04EMA16S in a NEMA 4 SS enclosure) and the SSP04EMA16 is UL1449 5th edition listed.


CTA-ID : 2053576

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings