Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is the motor power scaled on an ATV61 / ATV71 analog output?
Issue:
Scaling of motor power on ATV61 / ATV71 AO1.

Product Line:
ATV61

Environment:
Analog output

Cause:
n/a

Resolution:
It is scaled from 0 to 2.5 times the Rated Motor Power (nPr), as set in the Simply Start or Motor control menus.