How can we help you today?

what if the ATV31 is giving the error message " SLF " and is not running ?

If the drive is controlled via a remote terminal unit, this error message appears when the Modbus cable is disconnected or damaged.
You have to check the cable in this case .