Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between onload and off load switch disconnectors and what is the type of INS switch ?
- On load switch disconnector:
it is switch disconnector that can open and close the circuit on load and perform the isolation required.

- Off Load switch disconnector:
It is switch disconnector that must open and close the circuit when load is off (it can not operate on nominal load) - For example - Earthing switch used with CB during maintenance

- The INS Switch is ON load type